Imx6 CSI multichannel video support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Imx6 CSI multichannel video support

2,068件の閲覧回数
abeeshmp_dct
Contributor II

Does IPU CSI has support for time multiplex BT656 video?

ラベル(5)
タグ(2)
0 件の賞賛
返信
3 返答(返信)

1,897件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi ABEESH

IPU parallel CSI can receive only one stream, if it contains

data from several sensors (channels) it should be parsed in

software.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,897件の閲覧回数
abeeshmp_dct
Contributor II

Hi Igor,

Thanks for the quick reply.

In my case, Video is coming from Pericom video decoder in BT656 TDM format, and it is connected to IPU0 CSI0.

CSI0/IDMAC can detect the BT656 TDM format to get video data to DDR ?

In my understanding, CSI0/IDMAC should get Embedded sync to get video data into DDR. In BT656 TDM format embedded sync is arranged in a different way than in normal BT656.

0 件の賞賛
返信

1,897件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi ABEESH

CSI hardware can recognize only normal BT656.

~-igor

0 件の賞賛
返信