Issue on PCIE REFCLK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
4,120件の閲覧回数
x10
Contributor V

Hi, NXP

A Si52112-B3 pcie clock generator is used in my iMX7D based board with Linux-4.9.11 kernel. 100MHz PCIE_REFCLKIN_P/N waveform is shown as follows:

20181017-ESM7100-4-Si52112-B4-PCIECLK-R26-1.png

After kernel booting up, I got following message about pcie driver loading:

20181017-ESM7100-pcie-driver-msg.JPG

As my understood, PCIE_PHY is not work properly, but can not figure out what issue with it.

It's appreciated for any help about this issue. Thanks!

BTW, the same kernel can run on iMX7D Sabre Board, and PCIE interface works fine with NVMe module.

BR

Cheng Shi

Emtronix

ラベル(2)
0 件の賞賛
返信
1 解決策
3,864件の閲覧回数
x10
Contributor V

PCIe is working with NMVe module in my customized iMX7D board. The problem is the PCMIC not set properly. Both Si5112-B3 and Si5112-B4 are okay. PCIE_REFCLK going through with 0R instead of 0.1uF is required.

BR

Cheng Shi

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
3,865件の閲覧回数
x10
Contributor V

PCIe is working with NMVe module in my customized iMX7D board. The problem is the PCMIC not set properly. Both Si5112-B3 and Si5112-B4 are okay. PCIE_REFCLK going through with 0R instead of 0.1uF is required.

BR

Cheng Shi

0 件の賞賛
返信
3,865件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Cheng 

one can look at suggestions provided for similar issue on

PCI Express PLL cannot lock on about 5% of all IMX7D CPUs. 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
3,865件の閲覧回数
x10
Contributor V

Thanks Igor for quick reply. I'll check my design about power supply with reference of your link.

BR

Cheng Shi

0 件の賞賛
返信