Issue on Camera: Multiple Frames on single screen

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Issue on Camera: Multiple Frames on single screen

1,932 次查看
aravinthkumarja
Senior Contributor II

Hi All,

We are using OV5647 MIPI camera on imx6 platform with Android 7.1.2 BSP. We have bring-up the camera on linux level and it's working perfectly on sample linux test application (mxc_v4l2_capture). Then I integrated this camera support on Android HAL. Now I'm able to view the camera data on default android application. But we are getting same camera data in 20 frames in a single screen, I have attached screenshot of captured image.

Can you please support on this.?

Regards,

Aravinth

0 项奖励
回复
1 回复

1,760 次查看
diegoadrian
NXP Employee
NXP Employee

Hello,

Unfortunately, the camera OV5467 is not supported by our BSP. However, you can try to use the OV5460 model. 

I apologize for the inconveniences.

Best Regards,

Diego.

0 项奖励
回复