Issue:/dev doesnot contain any mmc related partitions

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Issue:/dev doesnot contain any mmc related partitions

ソリューションへジャンプ
2,722件の閲覧回数
kpoojari7
Contributor I

Hello All,

 

I have successfully build and booted linux kernel on imx233 via NAND flash.

Now I wanted to mount SD card on it. However I am not able to find any mmc files in /dev folder of the booted kernel.

I have already enabled the following MMC related configuration symbols while building kernel:

 

#

# OTG and related infrastructure

#

CONFIG_USB_OTG_UTILS=y

# CONFIG_USB_GPIO_VBUS is not set

# CONFIG_NOP_USB_XCEIV is not set

# CONFIG_MXC_OTG is not set

CONFIG_MMC=y

CONFIG_MMC_DEBUG=y

CONFIG_MMC_UNSAFE_RESUME=y

 

#

# MMC/SD/SDIO Card Drivers

#

CONFIG_MMC_BLOCK=y

CONFIG_MMC_BLOCK_BOUNCE=y

CONFIG_SDIO_UART=y

CONFIG_MMC_TEST=y

 

#

# MMC/SD/SDIO Host Controller Drivers

#

CONFIG_MMC_SDHCI=y

CONFIG_MMC_SDHCI_PLTFM=y

CONFIG_MMC_SPI=y

CONFIG_MMC_IMX_ESDHCI_PIO_MODE=y

CONFIG_MMC_MXS=y

# CONFIG_MEMSTICK is not set

# CONFIG_ACCESSIBILITY is not set

# CONFIG_NEW_LEDS is not set

CONFIG_RTC_LIB=y

CONFIG_RTC_CLASS=y

CONFIG_RTC_HCTOSYS=y

CONFIG_RTC_HCTOSYS_DEVICE="rtc0"

# CONFIG_RTC_DEBUG is not set

 

Please help me in this regard.

I have attached the completed configuration also.

 

Thanks in advance

 

Regards,

Venkatesh

Original Attachment has been moved to: imx23evk_defconfig.dev.zip

タグ(4)
0 件の賞賛
返信
1 解決策
2,510件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Venkatesh

please refer to sect.22.5 Menu Configuration Options

attached document and L2.6.31_10.05.00_SDK_SOURCE : Linux 2.6.31

Source Code Files.

Note gpmi (nand) are used also for ssp2 interface, iMX23 EVK uses ssp1.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,511件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Venkatesh

please refer to sect.22.5 Menu Configuration Options

attached document and L2.6.31_10.05.00_SDK_SOURCE : Linux 2.6.31

Source Code Files.

Note gpmi (nand) are used also for ssp2 interface, iMX23 EVK uses ssp1.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,510件の閲覧回数
kpoojari7
Contributor I

Hello igorpadykov,

I have changed the command line argument with ssp1=mmc and it worked.

Thanks It worked.

0 件の賞賛
返信