Hello All,
I have successfully build and booted linux kernel on imx233 via NAND flash.
Now I wanted to mount SD card on it. However I am not able to find any mmc files in /dev folder of the booted kernel.
I have already enabled the following MMC related configuration symbols while building kernel:
#
# OTG and related infrastructure
#
CONFIG_USB_OTG_UTILS=y
# CONFIG_USB_GPIO_VBUS is not set
# CONFIG_NOP_USB_XCEIV is not set
# CONFIG_MXC_OTG is not set
CONFIG_MMC=y
CONFIG_MMC_DEBUG=y
CONFIG_MMC_UNSAFE_RESUME=y
#
# MMC/SD/SDIO Card Drivers
#
CONFIG_MMC_BLOCK=y
CONFIG_MMC_BLOCK_BOUNCE=y
CONFIG_SDIO_UART=y
CONFIG_MMC_TEST=y
#
# MMC/SD/SDIO Host Controller Drivers
#
CONFIG_MMC_SDHCI=y
CONFIG_MMC_SDHCI_PLTFM=y
CONFIG_MMC_SPI=y
CONFIG_MMC_IMX_ESDHCI_PIO_MODE=y
CONFIG_MMC_MXS=y
# CONFIG_MEMSTICK is not set
# CONFIG_ACCESSIBILITY is not set
# CONFIG_NEW_LEDS is not set
CONFIG_RTC_LIB=y
CONFIG_RTC_CLASS=y
CONFIG_RTC_HCTOSYS=y
CONFIG_RTC_HCTOSYS_DEVICE="rtc0"
# CONFIG_RTC_DEBUG is not set
Please help me in this regard.
I have attached the completed configuration also.
Thanks in advance
Regards,
Venkatesh
Original Attachment has been moved to: imx23evk_defconfig.dev.zip
解決済! 解決策の投稿を見る。
Hi Venkatesh
please refer to sect.22.5 Menu Configuration Options
attached document and L2.6.31_10.05.00_SDK_SOURCE
: Linux 2.6.31
Source Code Files.
Note gpmi (nand) are used also for ssp2 interface, iMX23 EVK uses ssp1.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Venkatesh
please refer to sect.22.5 Menu Configuration Options
attached document and L2.6.31_10.05.00_SDK_SOURCE
: Linux 2.6.31
Source Code Files.
Note gpmi (nand) are used also for ssp2 interface, iMX23 EVK uses ssp1.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello igorpadykov,
I have changed the command line argument with ssp1=mmc and it worked.
Thanks It worked.