Issue bitbaking qtdeclarative-native

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Issue bitbaking qtdeclarative-native

ソリューションへジャンプ
3,632件の閲覧回数
khang_letruong
Senior Contributor III

Hello,

I am struggling with the bitbaking of imx-image-full for iMX8M Plus with BSP LF-5.15.71-2-2.0. Specifically, it's stuck with the bitkaking of qtdeclarative-native package. Then I tried bitbake qtdeclarative-native -c cleanall && bitbake qtdeclarative-native -c compile but the issue continues happening :

| /workdir/polyhex-debix-som-a-yocto-bsp-5_15_71-2_2_x/build-xwayland/tmp/work/x86_64-linux/qtdeclarative-native/6.3.2-r0/recipe-sysroot-native/usr/libexec/moc -DBUILDING_QT__ -DENABLE_ASSEMBLER_WX_EXCLUSIVE=1 -DENABLE_DFG_JIT=0 -DENABLE_DFG_JIT_UTILITY_METHODS=1 -DENABLE_JIT_CONSTANT_BLINDING=0 -DENABLE_LLINT=0 -DJS_EXPORT_PRIVATE= -DNDEBUG -DQT_ASCII_CAST_WARNINGS -DQT_BUILDING_QT -DQT_BUILD_QML_LIB -DQT_CORE_LIB -DQT_DEPRECATED_WARNINGS -DQT_DEPRECATED_WARNINGS_SINCE=0x060000 -DQT_DISABLE_DEPRECATED_BEFORE=0x050000 -DQT_MOC_COMPAT -DQT_NETWORK_LIB -DQT_NO_CAST_TO_ASCII -DQT_NO_DEBUG -DQT_NO_EXCEPTIONS -DQT_NO_FOREACH -DQT_NO_INTEGER_EVENT_COORDINATES -DQT_NO_JAVA_STYLE_ITERATORS -DQT_NO_NARROWING_CONVERSIONS_IN_CONNECT -DQT_NO_URL_CAST_FROM_STRING -DQT_QMLINTEGRATION_LIB -DQT_USE_QSTRINGBUILDER -DQml_EXPORTS -DWTFInvokeCrashHook=qmlWTFInvokeCrashHook -DWTFReportAssertionFailure=qmlWTFReportAssertionFailure -DWTFReportAssertionFailureWithMessage=qmlWTFReportAssertionFailureWithMessage -DWTFReportBacktrace=qmlWTFReportBacktrace -DWTF_EXPORT_PRIVATE= -DWTF_USE_UDIS86=0 -D_LARGEFILE64_SOURCE -D_LARGEFILE_SOURCE -I/workdir/polyhex-debix-som-a-yocto-bsp-5_15_71-2_2_x/build-xwayland/tmp/work/x86_64-linux/qtdeclarative-native/6.3.2-r0/build/include -I/workdir/polyhex-debix-som-a-yocto-bsp-5_15_71-2_2_x/build-xwayland/tmp/work/x86_64-linux/qtdeclarative-native/6.3.2-r0/build/include/QtQml -I/workdir/polyhex-debix-som-a-yocto-bsp-5_15_71-2_2_x/build-xwayland/tmp/work/x86_64-linux/qtdeclarative-native/6.3.2-r0/git/src/qml -I/workdir/polyhex-debix-som-a-yocto-bsp-5_15_71-2_2_x/build-xwayland/tmp/work/x86_64-linux/qtdeclarative-native/6.3.2-r0/build/src/qml -I/workdir/polyhex-debix-som-a-yocto-bsp-5_15_71-2_2_x/build-xwayland/tmp/work/x86_64-linux/qtdeclarative-native/6.3.2-r0/build/src/qml/compiler -I/workdir/polyhex-debix-som-a-yocto-bsp-5_15_71-2_2_x/build-xwayland/tmp/work/x86_64-linux/qtdeclarative-native/6.3.2-r0/build/src/qml/jsruntime -I/workdir/polyhex-debix-som-a-yocto-bsp-5_15_71-2_2_x/build-xwayland/tmp/work/x86_64-linux/qtdeclarative-native/6.3.2-r0/build/src/qml/memory -I/workdir/polyhex-debix-som-a-yocto-bsp-5_15_71-2_2_x/build-xwayland/tmp/work/x86_64-linux/qtdeclarative-native/6.3.2-r0/build/src/qml/qmldirparser -I/workdir/polyhex-debix-som-a-yocto-bsp-5_15_71-2_2_x/build-xwayland/tmp/work/x86_64-linux/qtdeclarative-native/6.3.2-r0/git/src/3rdparty/masm -I/workdir/polyhex-debix-som-a-yocto-bsp-5_15_71-2_2_x/build-xwayland/tmp/work/x86_64-linux/qtdeclarative-native/6.3.2-r0/git/src/3rdparty/masm/assembler -I/workdir/polyhex-debix-som-a-yocto-bsp-5_15_71-2_2_x/build-xwayland/tmp/work/x86_64-linux/qtdeclarative-native/6.3.2-r0/git/src/3rdparty/masm/disassembler -I/workdir/polyhex-debix-som-a-yocto-bsp-5_15_71-2_2_x/build-xwayland/tmp/work/x86_64-linux/qtdeclarative-native/6.3.2-r0/git/src/3rdparty/masm/disassembler/udis86 -I/workdir/polyhex-debix-som-a-yocto-bsp-5_15_71-2_2_x/build-xwayland/tmp/work/x86_64-linux/qtdeclarative-native/6.3.2-r0/git/src/3rdparty/masm/jit -I/workdir/polyhex-debix-som-a-yocto-bsp-5_15_71-2_2_x/build-xwayland/tmp/work/x86_64-linux/qtdeclarative-native/6.3.2-r0/git/src/3rdparty/masm/runtime -I/workdir/polyhex-debix-som-a-yocto-bsp-5_15_71-2_2_x/build-xwayland/tmp/work/x86_64-linux/qtdeclarative-native/6.3.2-r0/git/src/3rdparty/masm/stubs -I/workdir/polyhex-debix-som-a-yocto-bsp-5_15_71-2_2_x/build-xwayland/tmp/work/x86_64-linux/qtdeclarative-native/6.3.2-r0/git/src/3rdparty/masm/stubs/runtime -I/workdir/polyhex-debix-som-a-yocto-bsp-5_15_71-2_2_x/build-xwayland/tmp/work/x86_64-linux/qtdeclarative-native/6.3.2-r0/git/src/3rdparty/masm/stubs/wtf -I/workdir/polyhex-debix-som-a-yocto-bsp-5_15_71-2_2_x/build-xwayland/tmp/work/x86_64-linux/qtdeclarative-native/6.3.2-r0/git/src/3rdparty/masm/wtf -I/workdir/polyhex-debix-som-a-yocto-bsp-5_15_71-2_2_x/build-xwayland/tmp/work/x86_64-linux/qtdeclarative-native/6.3.2-r0/git/src/qml/.generated -I/workdir/polyhex-debix-som-a-yocto-bsp-5_15_71-2_2_x/build-xwayland/tmp/work/x86_64-linux/qtdeclarative-native/6.3.2-r0/git/src/qml/compiler -I/workdir/polyhex-debix-som-a-yocto-bsp-5_15_71-2_2_x/build-xwayland/tmp/work/x86_64-linux/qtdeclarative-native/6.3.2-r0/git/src/qml/debugger -I/workdir/polyhex-debix-som-a-yocto-bsp-5_15_71-2_2_x/build-xwayland/tmp/work/x86_64-linux/qtdeclarative-native/6.3.2-r0/git/src/qml/jsruntime -I/workdir/polyhex-debix-som-a-yocto-bsp-5_15_71-2_2_x/build-xwayland/tmp/work/x86_64-linux/qtdeclarative-native/6.3.2-r0/git/src/qml/memory -I/workdir/polyhex-debix-som-a-yocto-bsp-5_15_71-2_2_x/build-xwayland/tmp/work/x86_64-linux/qtdeclarative-native/6.3.2-r0/git/src/qml/qmldirparser -I/workdir/polyhex-debix-som-a-yocto-bsp-5_15_71-2_2_x/build-xwayland/tmp/work/x86_64-linux/qtdeclarative-native/6.3.2-r0/build/include/QtQml/6.3.3 -I/workdir/polyhex-debix-som-a-yocto-bsp-5_15_71-2_2_x/build-xwayland/tmp/work/x86_64-linux/qtdeclarative-native/6.3.2-r0/build/include/QtQml/6.3.3/QtQml -I/workdir/polyhex-debix-som-a-yocto-bsp-5_15_71-2_2_x/build-xwayland/tmp/work/x86_64-linux/qtdeclarative-native/6.3.2-r0/recipe-sysroot-native/usr/include/QtCore/6.3.3 -I/workdir/polyhex-debix-som-a-yocto-bsp-5_15_71-2_2_x/build-xwayland/tmp/work/x86_64-linux/qtdeclarative-native/6.3.2-r0/recipe-sysroot-native/usr/include/QtCore/6.3.3/QtCore -I/workdir/polyhex-debix-som-a-yocto-bsp-5_15_71-2_2_x/build-xwayland/tmp/work/x86_64-linux/qtdeclarative-native/6.3.2-r0/recipe-sysroot-native/usr/include/QtCore -I/workdir/polyhex-debix-som-a-yocto-bsp-5_15_71-2_2_x/build-xwayland/tmp/work/x86_64-linux/qtdeclarative-native/6.3.2-r0/recipe-sysroot-native/usr/lib/mkspecs/linux-g++ -I/workdir/polyhex-debix-som-a-yocto-bsp-5_15_71-2_2_x/build-xwayland/tmp/work/x86_64-linux/qtdeclarative-native/6.3.2-r0/build/include/QtQmlIntegration -I/workdir/polyhex-debix-som-a-yocto-bsp-5_15_71-2_2_x/build-xwayland/tmp/work/x86_64-linux/qtdeclarative-native/6.3.2-r0/git/src/qmlintegration -I/workdir/polyhex-debix-som-a-yocto-bsp-5_15_71-2_2_x/build-xwayland/tmp/work/x86_64-linux/qtdeclarative-native/6.3.2-r0/build/src/qmlintegration -I/workdir/polyhex-debix-som-a-yocto-bsp-5_15_71-2_2_x/build-xwayland/tmp/work/x86_64-linux/qtdeclarative-native/6.3.2-r0/recipe-sysroot-native/usr/include/QtNetwork -I/workdir/polyhex-debix-som-a-yocto-bsp-5_15_71-2_2_x/build-xwayland/tmp/work/x86_64-linux/qtdeclarative-native/6.3.2-r0/build/src/qml/.generated/release -I/workdir/polyhex-debix-som-a-yocto-bsp-5_15_71-2_2_x/build-xwayland/tmp/work/x86_64-linux/qtdeclarative-native/6.3.2-r0/build/src/qml/jit -I/workdir/polyhex-debix-som-a-yocto-bsp-5_15_71-2_2_x/build-xwayland/tmp/work/x86_64-linux/qtdeclarative-native/6.3.2-r0/git/src/qml/jit -I/workdir/polyhex-debix-som-a-yocto-bsp-5_15_71-2_2_x/build-xwayland/tmp/work/x86_64-linux/qtdeclarative-native/6.3.2-r0/git/src/qml/animations -I/workdir/polyhex-debix-som-a-yocto-bsp-5_15_71-2_2_x/build-xwayland/tmp/work/x86_64-linux/qtdeclarative-native/6.3.2-r0/recipe-sysroot-native/usr/include -I/usr/include/c++/9 -I/usr/include/x86_64-linux-gnu/c++/9 -I/usr/include/c++/9/backward -I/usr/lib/gcc/x86_64-linux-gnu/9/include -I/usr/local/include -I/usr/include/x86_64-linux-gnu -I/usr/include --include /workdir/polyhex-debix-som-a-yocto-bsp-5_15_71-2_2_x/build-xwayland/tmp/work/x86_64-linux/qtdeclarative-native/6.3.2-r0/build/src/qml/Qml_autogen/moc_predefs.h --output-json --output-dep-file -o /workdir/polyhex-debix-som-a-yocto-bsp-5_15_71-2_2_x/build-xwayland/tmp/work/x86_64-linux/qtdeclarative-native/6.3.2-r0/build/src/qml/Qml_autogen/include/moc_qqmlloggingcategory_p.cpp /workdir/polyhex-debix-som-a-yocto-bsp-5_15_71-2_2_x/build-xwayland/tmp/work/x86_64-linux/qtdeclarative-native/6.3.2-r0/git/src/qml/qml/qqmlloggingcategory_p.h
| 
| AutoMoc subprocess error
| ------------------------
| The moc process failed to compile
|   "SRC:/src/qml/qml/qqmlextensionplugin.h"
| into
|   "BIN:/src/qml/Qml_autogen/include/moc_qqmlextensionplugin.cpp"
| included by
|   "SRC:/src/qml/qml/qqmlextensionplugin.cpp"
| 
| Command
| -------
| /workdir/polyhex-debix-som-a-yocto-bsp-5_15_71-2_2_x/build-xwayland/tmp/work/x86_64-linux/qtdeclarative-native/6.3.2-r0/recipe-sysroot-native/usr/libexec/moc -DBUILDING_QT__ -DENABLE_ASSEMBLER_WX_EXCLUSIVE=1 -DENABLE_DFG_JIT=0 -DENABLE_DFG_JIT_UTILITY_METHODS=1 -DENABLE_JIT_CONSTANT_BLINDING=0 -DENABLE_LLINT=0 -DJS_EXPORT_PRIVATE= -DNDEBUG -DQT_ASCII_CAST_WARNINGS -DQT_BUILDING_QT -DQT_BUILD_QML_LIB -DQT_CORE_LIB -DQT_DEPRECATED_WARNINGS -DQT_DEPRECATED_WARNINGS_SINCE=0x060000 -DQT_DISABLE_DEPRECATED_BEFORE=0x050000 -DQT_MOC_COMPAT -DQT_NETWORK_LIB -DQT_NO_CAST_TO_ASCII -DQT_NO_DEBUG -DQT_NO_EXCEPTIONS -DQT_NO_FOREACH -DQT_NO_INTEGER_EVENT_COORDINATES -DQT_NO_JAVA_STYLE_ITERATORS -DQT_NO_NARROWING_CONVERSIONS_IN_CONNECT -DQT_NO_URL_CAST_FROM_STRING -DQT_QMLINTEGRATION_LIB -DQT_USE_QSTRINGBUILDER -DQml_EXPORTS -DWTFInvokeCrashHook=qmlWTFInvokeCrashHook -DWTFReportAssertionFailure=qmlWTFReportAssertionFailure -DWTFReportAssertionFailureWithMessage=qmlWTFReportAssertionFailureWithMessage -DWTFReportBacktrace=qmlWTFReportBacktrace -DWTF_EXPORT_PRIVATE= -DWTF_USE_UDIS86=0 -D_LARGEFILE64_SOURCE -D_LARGEFILE_SOURCE -I/workdir/polyhex-debix-som-a-yocto-bsp-5_15_71-2_2_x/build-xwayland/tmp/work/x86_64-linux/qtdeclarative-native/6.3.2-r0/build/include -I/workdir/polyhex-debix-som-a-yocto-bsp-5_15_71-2_2_x/build-xwayland/tmp/work/x86_64-linux/qtdeclarative-native/6.3.2-r0/build/include/QtQml -I/workdir/polyhex-debix-som-a-yocto-bsp-5_15_71-2_2_x/build-xwayland/tmp/work/x86_64-linux/qtdeclarative-native/6.3.2-r0/git/src/qml -I/workdir/polyhex-debix-som-a-yocto-bsp-5_15_71-2_2_x/build-xwayland/tmp/work/x86_64-linux/qtdeclarative-native/6.3.2-r0/build/src/qml -I/workdir/polyhex-debix-som-a-yocto-bsp-5_15_71-2_2_x/build-xwayland/tmp/work/x86_64-linux/qtdeclarative-native/6.3.2-r0/build/src/qml/compiler -I/workdir/polyhex-debix-som-a-yocto-bsp-5_15_71-2_2_x/build-xwayland/tmp/work/x86_64-linux/qtdeclarative-native/6.3.2-r0/build/src/qml/jsruntime -I/workdir/polyhex-debix-som-a-yocto-bsp-5_15_71-2_2_x/build-xwayland/tmp/work/x86_64-linux/qtdeclarative-native/6.3.2-r0/build/src/qml/memory -I/workdir/polyhex-debix-som-a-yocto-bsp-5_15_71-2_2_x/build-xwayland/tmp/work/x86_64-linux/qtdeclarative-native/6.3.2-r0/build/src/qml/qmldirparser -I/workdir/polyhex-debix-som-a-yocto-bsp-5_15_71-2_2_x/build-xwayland/tmp/work/x86_64-linux/qtdeclarative-native/6.3.2-r0/git/src/3rdparty/masm -I/workdir/polyhex-debix-som-a-yocto-bsp-5_15_71-2_2_x/build-xwayland/tmp/work/x86_64-linux/qtdeclarative-native/6.3.2-r0/git/src/3rdparty/masm/assembler -I/workdir/polyhex-debix-som-a-yocto-bsp-5_15_71-2_2_x/build-xwayland/tmp/work/x86_64-linux/qtdeclarative-native/6.3.2-r0/git/src/3rdparty/masm/disassembler -I/workdir/polyhex-debix-som-a-yocto-bsp-5_15_71-2_2_x/build-xwayland/tmp/work/x86_64-linux/qtdeclarative-native/6.3.2-r0/git/src/3rdparty/masm/disassembler/udis86 -I/workdir/polyhex-debix-som-a-yocto-bsp-5_15_71-2_2_x/build-xwayland/tmp/work/x86_64-linux/qtdeclarative-native/6.3.2-r0/git/src/3rdparty/masm/jit -I/workdir/polyhex-debix-som-a-yocto-bsp-5_15_71-2_2_x/build-xwayland/tmp/work/x86_64-linux/qtdeclarative-native/6.3.2-r0/git/src/3rdparty/masm/runtime -I/workdir/polyhex-debix-som-a-yocto-bsp-5_15_71-2_2_x/build-xwayland/tmp/work/x86_64-linux/qtdeclarative-native/6.3.2-r0/git/src/3rdparty/masm/stubs -I/workdir/polyhex-debix-som-a-yocto-bsp-5_15_71-2_2_x/build-xwayland/tmp/work/x86_64-linux/qtdeclarative-native/6.3.2-r0/git/src/3rdparty/masm/stubs/runtime -I/workdir/polyhex-debix-som-a-yocto-bsp-5_15_71-2_2_x/build-xwayland/tmp/work/x86_64-linux/qtdeclarative-native/6.3.2-r0/git/src/3rdparty/masm/stubs/wtf -I/workdir/polyhex-debix-som-a-yocto-bsp-5_15_71-2_2_x/build-xwayland/tmp/work/x86_64-linux/qtdeclarative-native/6.3.2-r0/git/src/3rdparty/masm/wtf -I/workdir/polyhex-debix-som-a-yocto-bsp-5_15_71-2_2_x/build-xwayland/tmp/work/x86_64-linux/qtdeclarative-native/6.3.2-r0/git/src/qml/.generated -I/workdir/polyhex-debix-som-a-yocto-bsp-5_15_71-2_2_x/build-xwayland/tmp/work/x86_64-linux/qtdeclarative-native/6.3.2-r0/git/src/qml/compiler -I/workdir/polyhex-debix-som-a-yocto-bsp-5_15_71-2_2_x/build-xwayland/tmp/work/x86_64-linux/qtdeclarative-native/6.3.2-r0/git/src/qml/debugger -I/workdir/polyhex-debix-som-a-yocto-bsp-5_15_71-2_2_x/build-xwayland/tmp/work/x86_64-linux/qtdeclarative-native/6.3.2-r0/git/src/qml/jsruntime -I/workdir/polyhex-debix-som-a-yocto-bsp-5_15_71-2_2_x/build-xwayland/tmp/work/x86_64-linux/qtdeclarative-native/6.3.2-r0/git/src/qml/memory -I/workdir/polyhex-debix-som-a-yocto-bsp-5_15_71-2_2_x/build-xwayland/tmp/work/x86_64-linux/qtdeclarative-native/6.3.2-r0/git/src/qml/qmldirparser -I/workdir/polyhex-debix-som-a-yocto-bsp-5_15_71-2_2_x/build-xwayland/tmp/work/x86_64-linux/qtdeclarative-native/6.3.2-r0/build/include/QtQml/6.3.3 -I/workdir/polyhex-debix-som-a-yocto-bsp-5_15_71-2_2_x/build-xwayland/tmp/work/x86_64-linux/qtdeclarative-native/6.3.2-r0/build/include/QtQml/6.3.3/QtQml -I/workdir/polyhex-debix-som-a-yocto-bsp-5_15_71-2_2_x/build-xwayland/tmp/work/x86_64-linux/qtdeclarative-native/6.3.2-r0/recipe-sysroot-native/usr/include/QtCore/6.3.3 -I/workdir/polyhex-debix-som-a-yocto-bsp-5_15_71-2_2_x/build-xwayland/tmp/work/x86_64-linux/qtdeclarative-native/6.3.2-r0/recipe-sysroot-native/usr/include/QtCore/6.3.3/QtCore -I/workdir/polyhex-debix-som-a-yocto-bsp-5_15_71-2_2_x/build-xwayland/tmp/work/x86_64-linux/qtdeclarative-native/6.3.2-r0/recipe-sysroot-native/usr/include/QtCore -I/workdir/polyhex-debix-som-a-yocto-bsp-5_15_71-2_2_x/build-xwayland/tmp/work/x86_64-linux/qtdeclarative-native/6.3.2-r0/recipe-sysroot-native/usr/lib/mkspecs/linux-g++ -I/workdir/polyhex-debix-som-a-yocto-bsp-5_15_71-2_2_x/build-xwayland/tmp/work/x86_64-linux/qtdeclarative-native/6.3.2-r0/build/include/QtQmlIntegration -I/workdir/polyhex-debix-som-a-yocto-bsp-5_15_71-2_2_x/build-xwayland/tmp/work/x86_64-linux/qtdeclarative-native/6.3.2-r0/git/src/qmlintegration -I/workdir/polyhex-debix-som-a-yocto-bsp-5_15_71-2_2_x/build-xwayland/tmp/work/x86_64-linux/qtdeclarative-native/6.3.2-r0/build/src/qmlintegration -I/workdir/polyhex-debix-som-a-yocto-bsp-5_15_71-2_2_x/build-xwayland/tmp/work/x86_64-linux/qtdeclarative-native/6.3.2-r0/recipe-sysroot-native/usr/include/QtNetwork -I/workdir/polyhex-debix-som-a-yocto-bsp-5_15_71-2_2_x/build-xwayland/tmp/work/x86_64-linux/qtdeclarative-native/6.3.2-r0/build/src/qml/.generated/release -I/workdir/polyhex-debix-som-a-yocto-bsp-5_15_71-2_2_x/build-xwayland/tmp/work/x86_64-linux/qtdeclarative-native/6.3.2-r0/build/src/qml/jit -I/workdir/polyhex-debix-som-a-yocto-bsp-5_15_71-2_2_x/build-xwayland/tmp/work/x86_64-linux/qtdeclarative-native/6.3.2-r0/git/src/qml/jit -I/workdir/polyhex-debix-som-a-yocto-bsp-5_15_71-2_2_x/build-xwayland/tmp/work/x86_64-linux/qtdeclarative-native/6.3.2-r0/git/src/qml/animations -I/workdir/polyhex-debix-som-a-yocto-bsp-5_15_71-2_2_x/build-xwayland/tmp/work/x86_64-linux/qtdeclarative-native/6.3.2-r0/recipe-sysroot-native/usr/include -I/usr/include/c++/9 -I/usr/include/x86_64-linux-gnu/c++/9 -I/usr/include/c++/9/backward -I/usr/lib/gcc/x86_64-linux-gnu/9/include -I/usr/local/include -I/usr/include/x86_64-linux-gnu -I/usr/include --include /workdir/polyhex-debix-som-a-yocto-bsp-5_15_71-2_2_x/build-xwayland/tmp/work/x86_64-linux/qtdeclarative-native/6.3.2-r0/build/src/qml/Qml_autogen/moc_predefs.h --output-json --output-dep-file -o /workdir/polyhex-debix-som-a-yocto-bsp-5_15_71-2_2_x/build-xwayland/tmp/work/x86_64-linux/qtdeclarative-native/6.3.2-r0/build/src/qml/Qml_autogen/include/moc_qqmlextensionplugin.cpp /workdir/polyhex-debix-som-a-yocto-bsp-5_15_71-2_2_x/build-xwayland/tmp/work/x86_64-linux/qtdeclarative-native/6.3.2-r0/git/src/qml/qml/qqmlextensionplugin.h
| 
| Output
| ------
| 
| 
| AutoMoc: Reading dependencies from "BIN:/src/qml/Qml_autogen/include/moc_qqmlglobal_p.cpp.d"
| AutoMoc: Reading dependencies from "BIN:/src/qml/Qml_autogen/include/moc_qqmllocale_p.cpp.d"
| AutoMoc: Reading dependencies from "BIN:/src/qml/Qml_autogen/include/moc_qqmlloggingcategory_p.cpp.d"
| ninja: build stopped: subcommand failed.
| WARNING: exit code 1 from a shell command.
ERROR: Task (virtual:native:/workdir/polyhex-debix-som-a-yocto-bsp-5_15_71-2_2_x/sources/meta-qt6/recipes-qt/qt6/qtdeclarative_git.bb:do_compile) failed with exit code '1'
NOTE: Tasks Summary: Attempted 472 tasks of which 464 didn't need to be rerun and 1 failed.

Summary: 1 task failed:
  virtual:native:/workdir/polyhex-debix-som-a-yocto-bsp-5_15_71-2_2_x/sources/meta-qt6/recipes-qt/qt6/qtdeclarative_git.bb:do_compile
Summary: There was 1 ERROR message, returning a non-zero exit code.

 

Build environment : Docker Ubuntu 20.04

 Could you advice, please ?

Thanks in advance and best regards,

Khang

0 件の賞賛
返信
1 解決策
3,576件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @khang_letruong 

Please try to delete the yocto build folder and then bitbake qtdeclarative-native separately

Best Regards

Zhiming

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
3,577件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @khang_letruong 

Please try to delete the yocto build folder and then bitbake qtdeclarative-native separately

Best Regards

Zhiming

0 件の賞賛
返信
3,569件の閲覧回数
khang_letruong
Senior Contributor III

Hi @Zhiming_Liu ,

I confirm that I was able to avoid the issue after re-launching a multiple of times of the bitbake commands, including your suggestion, without modifying anything. Perhaps it was caused by the performance of the host machine on which the bitbake command is running.

Best Regards,

Khang

 

 

0 件の賞賛
返信