MAC Address for Windows 10 IoT

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MAC Address for Windows 10 IoT

1,101件の閲覧回数
hankwang
Contributor V

Hi,

      I have a MX8MP CPU and our MAC address needs to be written to the eeprom. Now, when the system goes into Windows, the i.MX Ethernet QoS Adapter fails to install the driver on the custom board. This is because the Ethernet QoS driver obtained the 00-00-00-00-00-00 MAC address.

      We want to read MAC address from the eeprom. Where do we need to modify?

     Please help us give some ideas. Thanks.

ラベル(1)
0 件の賞賛
返信
1 返信

1,049件の閲覧回数
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hello @hankwang,

I hope you are doing well.

Please find the engineering team response given below.

what they please mend by Eeprom. External I2C eeprom or SoC Fuses?

Windows 10 IoT BSP uses internal fuses as storage for MAC addresses. It is than read with help of ACPI method _DSM. In this method there could be made changes, if the MAC shall be read from different address. E.g. from a RAM location, where some external EEPROM service routine stored it previously.

Thanks & Regards,
Sanket Parekh

0 件の賞賛
返信