Issue about changing GPIO LVE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Issue about changing GPIO LVE

1,294件の閲覧回数
tony_l_cai
Contributor III

Hi,all

     I want to know how to change GPIO voltage 3.3v to 1.8v when its signal is "1" on i.MX6DL soc

and I know ,on i.MX6SL, we have a bit LVE, I can change the LVE=enable, then when signal is "1" the GPIO output 1.8v.

can you give me help,3Q!

ラベル(2)
0 件の賞賛
返信
1 返信

1,187件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi tony

i.MX6SDL GPIO cell has not LVE configuration,

GPIO IO parameters are given in Table 23. GPIO DC Parameters IMX6SDLCEC

so for changing GPIO voltage 3.3v to 1.8v one will have to change power supply

for appropriate power domain, check Table 100. 21 x 21 mm Functional Contact Assignments.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信