Issue about changing GPIO LVE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Issue about changing GPIO LVE

1,291 Views
tony_l_cai
Contributor III

Hi,all

     I want to know how to change GPIO voltage 3.3v to 1.8v when its signal is "1" on i.MX6DL soc

and I know ,on i.MX6SL, we have a bit LVE, I can change the LVE=enable, then when signal is "1" the GPIO output 1.8v.

can you give me help,3Q!

Labels (2)
0 Kudos
Reply
1 Reply

1,184 Views
igorpadykov
NXP Employee
NXP Employee

Hi tony

i.MX6SDL GPIO cell has not LVE configuration,

GPIO IO parameters are given in Table 23. GPIO DC Parameters IMX6SDLCEC

so for changing GPIO voltage 3.3v to 1.8v one will have to change power supply

for appropriate power domain, check Table 100. 21 x 21 mm Functional Contact Assignments.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply