Issue about Download mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Issue about Download mode

ソリューションへジャンプ
1,895件の閲覧回数
tony_l_cai
Contributor III

Hi,all

     I want to verify whether system is reset after I enter into serial downloader mode without pluging in the USB cable(this test is refer to the USB Boot Flow in i.mx6dl reference manual(p386)). As it said,if it didnt detect the usb  and WDOG_ENABLE =0, it would loop and not to reset.

     So, could you tell me, in this process, whether I can refer to  some log to know it how to work? such as log about reset and boot,the prompt during entering into serial download mode?

ラベル(3)
0 件の賞賛
返信
1 解決策
1,791件の閲覧回数
Yuri
NXP Employee
NXP Employee

  There is no any prompt during entering the serial boot mode.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,792件の閲覧回数
Yuri
NXP Employee
NXP Employee

  There is no any prompt during entering the serial boot mode.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信