Issue about Download mode

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Issue about Download mode

跳至解决方案
1,888 次查看
tony_l_cai
Contributor III

Hi,all

     I want to verify whether system is reset after I enter into serial downloader mode without pluging in the USB cable(this test is refer to the USB Boot Flow in i.mx6dl reference manual(p386)). As it said,if it didnt detect the usb  and WDOG_ENABLE =0, it would loop and not to reset.

     So, could you tell me, in this process, whether I can refer to  some log to know it how to work? such as log about reset and boot,the prompt during entering into serial download mode?

标签 (3)
0 项奖励
回复
1 解答
1,784 次查看
Yuri
NXP Employee
NXP Employee

  There is no any prompt during entering the serial boot mode.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,785 次查看
Yuri
NXP Employee
NXP Employee

  There is no any prompt during entering the serial boot mode.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复