Issue about DDR settings on Boot Config

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Issue about DDR settings on Boot Config

1,207 Views
tony_l_cai
Contributor III

Hi,all

     Our customize board is i.MX6DL,we use 4 pics of 16bit DDR3, so should we set the BOOT_CFG3[5:4]=10, which means

DDR Memory Map default config is "4KB Interleaving Enabled"?

     But I found, after we set DDR Memory Map default config as 00(Single DDR channel), it can work well. So could you give me more info about how to set this DDR boot config. 3Q!

Labels (2)
0 Kudos
Reply
1 Reply

1,082 Views
igorpadykov
NXP Employee
NXP Employee

Hi tony

"4KB Interleaving " mode is applicable only for LPDDR2 2-channels mode:

one channel for even 4K, other for odd 4K addresses.


Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------


0 Kudos
Reply