Is there i.MX6 Platform SDK for imx6ul?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is there i.MX6 Platform SDK for imx6ul?

1,566 Views
dongpv
Contributor III

Hello,

Currently, We are developing our product base on imx6ul. with previous versions, I used i.MX6 Series Platform SDK version 1.1 to test our customize board using imx6dual and imx6dualLite but with this version, I can't find sdk and library for imx6ul. Could you please share me know where I can find this software?

Many Thanks,

Dong

Labels (1)
0 Kudos
Reply
3 Replies

1,197 Views
igorpadykov
NXP Employee
NXP Employee

Hi Dong

unfortunately for i.MX6UL SDK was not released.

However since many modules are the same as for i.MX6DQ/SDL

in general it can be reused for it.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,197 Views
dongpv
Contributor III

Hi igor,

Thanks for your respond. I will try with your solution.

But I'm worry about address of register will be difference between imx6ul and  imx6DQ/SDL .

Do we need do some that changes before reused it?

As I know, In previous version, I can't reuse library from imx6DQ for imx6solo/dualLite then I have to library properly for imx6DSL.

Best Regards,

Dong

0 Kudos
Reply

1,197 Views
igorpadykov
NXP Employee
NXP Employee

Hi Dong

 

yes addresses should be changed for i.MX6UL.

Best regards

igor

0 Kudos
Reply