Is there any idea to use both ENET2 and EIM simultaneously for i.MX7D?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Is there any idea to use both ENET2 and EIM simultaneously for i.MX7D?

跳至解决方案
1,393 次查看
torus1000
Contributor V

Hi,

I checked i.MX7D pins with PinTool v.4.0 then found conflictions between ENET2(RGMII2) and EIM(AD21-10).

In this case, very restricted address pins were availabe for EIM such as {A27-A22,A9-A0}.
If I changed the mode from RGMII to RMII, 4 more pins could be available as following.

{A27-A22,A19,A18,A13,A12,A9-A0}

Obviously it is not convenient for me anyway because I need to access 8Mb SRAM thru EIM.

How can I avoid this conflictions; ENET2(RGMII2) and EIM(AD21-10)?

Is there any idea to use both ENET2 and EIM simultaneously?

Can anyone help me?

标签 (1)
0 项奖励
回复
1 解答
1,252 次查看
Yuri
NXP Employee
NXP Employee

Hello,

 

  As I see, it is not possible to configure i.MX7 for Your purposes, since some RGMII2

and EIM signals have only single (conflicting) multiplexing option. Look at section 8.1.1.1

(Muxing Options) of the i.MX7D RM (Rev. 1, 01/2018).


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,253 次查看
Yuri
NXP Employee
NXP Employee

Hello,

 

  As I see, it is not possible to configure i.MX7 for Your purposes, since some RGMII2

and EIM signals have only single (conflicting) multiplexing option. Look at section 8.1.1.1

(Muxing Options) of the i.MX7D RM (Rev. 1, 01/2018).


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复