Is there a web server which provide imx RPMs ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is there a web server which provide imx RPMs ?

1,562件の閲覧回数
rans
Senior Contributor I

Hello,

I read some tutorial in this forum about making your PC as a web server for rpm.

But Isn't there any web server in www , which can be used for this purpose ?

Thank you!

Ran

0 件の賞賛
返信
2 返答(返信)

1,463件の閲覧回数
b36401
NXP Employee
NXP Employee

You can use some light web server like nginx for such purposes.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,463件の閲覧回数
rans
Senior Contributor I

Hi Victor,

I am looking for the simplicity of connecting target to internet, and using "yum" or "apt-get".

For some reason, I don't see there is a good solution in yocto for online package installation.

On the other hand,  If I install debian with imx6, it should work, Right ?

Regards,

Ran

0 件の賞賛
返信