Is there a web server which provide imx RPMs ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is there a web server which provide imx RPMs ?

1,491 Views
rans
Senior Contributor I

Hello,

I read some tutorial in this forum about making your PC as a web server for rpm.

But Isn't there any web server in www , which can be used for this purpose ?

Thank you!

Ran

0 Kudos
Reply
2 Replies

1,392 Views
b36401
NXP Employee
NXP Employee

You can use some light web server like nginx for such purposes.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,392 Views
rans
Senior Contributor I

Hi Victor,

I am looking for the simplicity of connecting target to internet, and using "yum" or "apt-get".

For some reason, I don't see there is a good solution in yocto for online package installation.

On the other hand,  If I install debian with imx6, it should work, Right ?

Regards,

Ran

0 Kudos
Reply