Is there a way to change start-up sequence of PF3001?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Is there a way to change start-up sequence of PF3001?

跳至解决方案
1,689 次查看
durmus
Contributor IV


Hello everyone,

My custom board with iMX6UL just arrived and it is not detected by PC (via USB). I checked boot switches, voltage levels, etc. After some more investigation, I think power-up sequence might be the problem.

I use PF3001 with A7 option in my design. VDD_HIGH_IN is connected to SW2 output and VDD_SOC_IN is connected to SW1 output. I realized that datasheet says VDD_HIGH_IN must be powered before VDD_SOC_IN. However, in PF3001 A7 configuration, SW1 and SW2 have the same sequence number, which is 3.

If really that is the problem, what I want to do is to change start-up sequence so that SW2 is ready before SW1 is turned on. I realize that V33 output could have beed used for VDD_HIGH_IN. But right now, that is not an option.

PF100 has this TBB (try before buy) feature to allow changing start-up sequence. PF3001 datasheet does not mention it, but is there any way to change start-up sequence of PF3001?

Thanks.

标签 (1)
标记 (4)
0 项奖励
回复
1 解答
1,250 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Durmuş

as described in sect.1 Orderable parts :

"The PF3001 is available with pre-programmed OTP memory configurations."

so seems there is no way to change power-up sequence or use TBB prototyping mode.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,251 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Durmuş

as described in sect.1 Orderable parts :

"The PF3001 is available with pre-programmed OTP memory configurations."

so seems there is no way to change power-up sequence or use TBB prototyping mode.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复