Is it possible to write eMMC with 'dd' command in linux?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is it possible to write eMMC with 'dd' command in linux?

Jump to solution
4,611 Views
JHY
Contributor IV

I use i.MX6 SABRE-SDP board.

I want to know whether writing eMMC is possible after booting from SD card slot or NFS.

Thank you.

Labels (1)
0 Kudos
Reply
1 Solution
3,760 Views
igorpadykov
NXP Employee
NXP Employee

Hi JHY

yes it is possible, for example attached Linux Guide sect.8.3

shows such operations for both SD/eMMC.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
3,761 Views
igorpadykov
NXP Employee
NXP Employee

Hi JHY

yes it is possible, for example attached Linux Guide sect.8.3

shows such operations for both SD/eMMC.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply