Is it possible to write eMMC with 'dd' command in linux?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is it possible to write eMMC with 'dd' command in linux?

ソリューションへジャンプ
4,579件の閲覧回数
JHY
Contributor IV

I use i.MX6 SABRE-SDP board.

I want to know whether writing eMMC is possible after booting from SD card slot or NFS.

Thank you.

ラベル(1)
0 件の賞賛
返信
1 解決策
3,728件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi JHY

yes it is possible, for example attached Linux Guide sect.8.3

shows such operations for both SD/eMMC.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
3,729件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi JHY

yes it is possible, for example attached Linux Guide sect.8.3

shows such operations for both SD/eMMC.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信