Is it possible to verify keys using kobs-ng?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is it possible to verify keys using kobs-ng?

950件の閲覧回数
JohnKlug
Senior Contributor I
I concatenated the first 4 fuse words of the fuse bank (not sure what is expected here):

root@imx6ull14x14evk:~# kobs-ng  imgverify -v -kF315B19099EF27C626B10686ABDD61DC  u-boot-nand-signed.imx
u-boot-nand-signed.imx: verifying using key 'f315b19099ef27c626b10686abdd61dc'
u-boot-nand-signed.imx: is a valid bootstream for key 'f315b19099ef27c626b10686abdd61dc'

 

I add one to the key, and it still works:

root@imx6ull14x14evk:~# kobs-ng  imgverify -v -kF315B19099EF27C626B10686ABDD61DD  u-boot-nand-signed.imx                                 
u-boot-nand-signed.imx: verifying using key 'f315b19099ef27c626b10686abdd61dd'
u-boot-nand-signed.imx: is a valid bootstream for key 'f315b19099ef27c626b10686abdd61dd'

 

 

ラベル(3)
0 件の賞賛
返信
1 返信

931件の閲覧回数
Yuri
NXP Employee
NXP Employee

@JohnKlug 
Hello,

   What kobs-ng release is used in the case?

Is it possible to try the recent one?

https://github.com/NXPmicro/imx-kobs

 

Regards,
Yuri.

0 件の賞賛
返信