Is it possible to implement hot-plug in IPU CSI

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is it possible to implement hot-plug in IPU CSI

1,115 Views
zohanlin
Contributor IV

Dear all

I used imx6q and BSP is 4.2.2, kernel version is 3.0.35.

I set CSI by BT.656 mode.

I plug video cable and use CSI to receive the video,

the video showed on LCD is OK.

But when I unplug the cable and plug it again, vsync function seems ineffective.

I think IPU CSI only do vsync function at the beginning of receiving video streaming, 

and it wouldn't do vsync function again when video cable is replugged.

is that right?

If it's right,  is it possible to make IPU CSI do vsync when video cable is replugged or implement hot-plug in IPU CSI ?

Thanks a lot,

zohan

0 Kudos
Reply
2 Replies

953 Views
igorpadykov
NXP Employee
NXP Employee

Hi zohan

I am afraid it is not possible to implement hot-plug in IPU CSI,

also resyncing function may not automatically work when video cable is replugged.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

953 Views
zohanlin
Contributor IV

Hi igor

Thanks for your answer.

It seems that I need to reload driver to sync again when I replug video table.

0 Kudos
Reply