How to verify IMX6 DualLite PCIe eye-diagram analyzsis

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to verify IMX6 DualLite PCIe eye-diagram analyzsis

737 Views
csfttl
Contributor I

Hi,

We need to verify PCIe eye-diagram on IMX6 DualLite, we refer "PCIe Certification Guide" (www.nxp.com/files/32bit/doc/app_note/AN4784.pdf) and found some problems.


1. About software setup, refer https://community.nxp.com/docs/DOC-94923

    This software patch & kernel config setting is too old, we can't apply it to Yocto-L3.14.38 BSP.

    Do you have new patch to modify "pic-imx6.c" for keep PCIe clock and power in the tests??

2. About hardware setup, do you have more detail document for us refer ??

    (like http://www.nxp.com/assets/documents/data/en/application-notes/AN5158.pdf)

Thanks,

Arthur

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

535 Views
b36401
NXP Employee
NXP Employee

No. We have no more recent pic-imx6.c.
Sorry for the inconvenience.

You can refer to chapter 2. "Test equipment" of noted Certification Guide regarding to hardware setup.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply