Is it possible to enable iMX6UL's EPIT in STOP mode?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is it possible to enable iMX6UL's EPIT in STOP mode?

Jump to solution
1,806 Views
kevinroussel
Contributor II

Hello,

I am optimizing the power consumption of an embedded device based on the iMX6UL processor. My aim is to leave it sleeping as long as possible, using the EPIT to wake it up regularly as needed.

Currently, I am able (thanks to a custom Linux kernel module) to use EPIT interrupts to wake up my system from WAIT mode. But power consumption in WAIT mode is still quite high for my purposes.

Thus, is there a wait to keep EPIT enable in STOP mode on the iMX6UL?

(According to the processor manual (CCM chapter), programming the CCGR1 register allows to keep EPIT clocks running only in run and WAIT mode. Similarly, setting the MOD_EN_OV_EPIT bit in CMEOR register doesn't seem to have any effect.)

Thanks in advance for any comment or advice,

Labels (2)
0 Kudos
Reply
1 Solution
1,726 Views
kevinroussel
Contributor II

Hello Igor,

Thanks for your answer. I forgot to state that I did set the STOPEN bit in the EPITx_CR register.

In the meantime, I found the answer to my problem: I configured the EPIT with the standard peripheral clock (putting 1 in CLKSRC field of EPITx_CR register), while this clock is disabled in STOP mode. I thus switched to the reference low-frequency clock (putting 3 in CLKSRC field of EPITx_CR register); this solved my problem, I can now use EPIT to wake up my system from STOP mode after a given delay.

Best regards,

View solution in original post

0 Kudos
Reply
2 Replies
1,726 Views
igorpadykov
NXP Employee
NXP Employee

Hi Kévin

one can check bit STOPEN in register EPITx_CR and description in

sect.23.4.3.2 Low-Power Mode Behavior i.MX6UL Reference Manual

http://www.nxp.com/docs/en/reference-manual/IMX6ULRM.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,727 Views
kevinroussel
Contributor II

Hello Igor,

Thanks for your answer. I forgot to state that I did set the STOPEN bit in the EPITx_CR register.

In the meantime, I found the answer to my problem: I configured the EPIT with the standard peripheral clock (putting 1 in CLKSRC field of EPITx_CR register), while this clock is disabled in STOP mode. I thus switched to the reference low-frequency clock (putting 3 in CLKSRC field of EPITx_CR register); this solved my problem, I can now use EPIT to wake up my system from STOP mode after a given delay.

Best regards,

0 Kudos
Reply