Is it possible to debug i.mx8x with gdb debugger running on windows host?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is it possible to debug i.mx8x with gdb debugger running on windows host?

1,309 Views
anaseem
Contributor IV

MCIM X8QXP-CPU evaluation board is running embedded Linux.  Is it possible to debug with gdb debugger running on windows host?

Tags (1)
0 Kudos
Reply
2 Replies

1,201 Views
igorpadykov
NXP Employee
NXP Employee

Hi Amer

one can check below link which may be helpful

How to JTAG debug iMX8mq? 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,201 Views
anaseem
Contributor IV

Or can embedded Linux target be debugged from gdb debugger running from terminal that is connected to Linux Server?

0 Kudos
Reply