Is it possible to capture MIPI-DSI output by the MIPI-CSI2 input?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is it possible to capture MIPI-DSI output by the MIPI-CSI2 input?

3,546 Views
ivannikolaenko
Contributor IV

Hello.

We have a device that outputs image to MIPI-DSI display. Is it possible (theoretically) to capture information from those device's MIPI-DSI by the MIPI-CSI2 input on the i.MX6Q?

Thank you.

Labels (4)
Tags (2)
0 Kudos
Reply
1 Reply

2,554 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ivan

it is possible to connect them since both use a similar phy, but I am afraid

no data can be received, as controllers use different specific protocols, such as

Camera (CSI) and Display (DSI). Some review is given at

http://rfmw.em.keysight.com/mod/pdf/axie_u4421a_mipi_d-phy_protocol_fundamentals_detailed_presentati...

Also it may be useful to post this on MIPI Alliance Contact Form | MIPI Alliance

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------