Hello,
I'd like to use two 1080p HDMI displays simultaneously, one connected directly to HDMI and the other to LCD through ADV7513.
I've also read About 1080p with LCD output on MX6Q and wanted to know if picture quality will be the same on both displays or LCD interface will produce worse picture?
In that thread there is information about poor LCD signal quality.
Is it still true? And if it is true will the upcoming SCM-i.MX6D resolve this issue?
Thanks!
Hi Yevhen
from theory point of view picture quality should be the same
but since such configuration was not tested on FSL reference boards,
it is not possible to say how it works in real application.
It may be suggested to ask people who performed such job on their boards.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------