Is it possible to build Yocto Project using remote Linux Server?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is it possible to build Yocto Project using remote Linux Server?

ソリューションへジャンプ
3,433件の閲覧回数
anaseem
Contributor IV

I need to build Yocto Project and load image into SD card.  Is it possible to use remote Linux server to build Yocto Project?  I will access Linux server from secure terminal running in my windows PC.  If yes, how will I load built image into SD card because Linux server is in remote location.

ラベル(1)
タグ(1)
1 解決策
3,281件の閲覧回数
radhikasomaiya
Senior Contributor II

Hi Amer Naseem,

It is possible to use remote Linux server to build Yocto Project. To load/flash compiled sdcard image, you need to transfer that image to your windows PC from remote server. Then you can load the image to sdcard.

Regards,

Radhika Somaiya.

元の投稿で解決策を見る

3 返答(返信)
3,282件の閲覧回数
radhikasomaiya
Senior Contributor II

Hi Amer Naseem,

It is possible to use remote Linux server to build Yocto Project. To load/flash compiled sdcard image, you need to transfer that image to your windows PC from remote server. Then you can load the image to sdcard.

Regards,

Radhika Somaiya.

3,281件の閲覧回数
anaseem
Contributor IV

How to load 'fsl-image-validation-imx' image into sdcard?  This image is specified on page 8 of i.MX Yocto Project User's Guide.

Documents talk about loading image onto an SD card using Linux dd command.  Instead, is it possible to transfer SD card image(.sdcard) to windows computer and then how to load/flash this image to SD card?

Regards,

Amer

0 件の賞賛
返信
3,281件の閲覧回数
anaseem
Contributor IV

Balena Etcher tool worked for loading/flashing Linux image into SD card from windows PC.  This tool is easy to use.

0 件の賞賛
返信