Generally, it seems to be possible to apply an external 24MHz clock signal
to XTALI and leave XTALO open, however, the amplitude of an external clock
signal must not exceed VDDXTAL, that is typically around 1.0V.
Next, an external oscillator may be connected to XTALO pin instead of XTALI pin. In addition,
an AC coupling capacitor should be place close to the i.MX28 so that the internal bias of the
i.MX28 circuit will not be affected.
However, this configuration is not recommended in practice. The XTALO as input is a high-impedance
one and therefore it increases noisy environment of the whole i.MX28, including the DCDC converters.