I downloaded the latest image IMX6_DQ_SDP_SD_DEMO_IMAGE (MX6Q-SDP-Android_r13.4.1.exe).
Since there are no install instructions, I just ran the executable on my WINXP system. After
burning the images onto a 16G SD card, I plugged the card into my platform and applied power. The image
does not boot and I do not see any UART activity. Plugging in the original SD card that came with our system works.
- Is there anything I need to know about prior to running the EXE such as format?
- Are there any limitations as to what type of card I can use to boot with (8G, HC, SANDISK-only)?
Solved! Go to Solution.
It turns out I was pointing to the logical drive and not the physical drive of my SD card. Selecting the physical driver fixed my issue.
It turns out I was pointing to the logical drive and not the physical drive of my SD card. Selecting the physical driver fixed my issue.