Is TDM Audio configuration only available for SAI1 in i.MX8mq processors?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Is TDM Audio configuration only available for SAI1 in i.MX8mq processors?

1,587 次查看
gabrielrivas
Contributor I

Just a simple question according to the i.MX8mq to confirm the information from the manual, for example if I need to share a SAI bus between 2 or more CODEC ICs, in a TDM configuration, the only way to do this is by using the SAI1?

Thanks

0 项奖励
回复
2 回复数

1,571 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Gabriel,

There is PCM in below section 3.5

https://www.nxp.com/docs/en/application-note/AN12202.pdf

And it's also mentioned in below community

https://community.nxp.com/thread/524538

Regards

 

0 项奖励
回复

1,553 次查看
gabrielrivas
Contributor I

Hi, thanks for your response. I had a look at the documentation you make reference and I had seen some responses on the support forums like : https://community.nxp.com/t5/i-MX-Processors/How-to-setup-sai1-tdm-mode-for-imx8mq-evk/m-p/888020

In the documentation they mention that in order to transfer several channels ( not clear if data or audio channels) you need to configure the bit fields TCE[] or RCE[] for Tx or Rx respectively. In the i.mx8 reference manual section 13.10 it says that this bit fields have to be set, but seems like only for the SAI1 it allows multiple channels, for any other SAI module it only allows 1 channel. I think I need more clarification on how to setup all the registers for TDM.

0 项奖励
回复