Is SPL still not supported in uboot-imx?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is SPL still not supported in uboot-imx?

Jump to solution
2,366 Views
noorahmadshinwa
Contributor III

Hi!

I am trying to build u-boot with HAB support for a custom board, and I am very confused. I would appreciate any support anyone could provide here.

I keep reading on other questions on this forum how the (official) nxp uboot-imx does not support SPL. I cloned what i think is the nxp uboot-imx from here:

git://source.codeaurora.org/external/imx/uboot-imx.git

branch=lf-5.4.y_v2019.04

When I look at the files for mx6sabresd, it sure looks like this version does support and build SPL by default.

Did the official nxp uboot-imx start supporting SPL or did i clone the wrong repo?

Thank you.

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
2,300 Views
igorpadykov
NXP Employee
NXP Employee

Hi Noorahmadshinwari

latest nxp uboot releases from source.codeaurora.org/external/imx/uboot-imx support spl.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
2,301 Views
igorpadykov
NXP Employee
NXP Employee

Hi Noorahmadshinwari

latest nxp uboot releases from source.codeaurora.org/external/imx/uboot-imx support spl.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
2,300 Views
noorahmadshinwa
Contributor III

Hi Igor,

Thank you for your response.

I would appreciate it if you could have a look at my related question here:

https://community.nxp.com/message/1346580 

Thanks again!

0 Kudos
Reply