Is SPL still not supported in uboot-imx?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Is SPL still not supported in uboot-imx?

跳至解决方案
2,489 次查看
noorahmadshinwa
Contributor III

Hi!

I am trying to build u-boot with HAB support for a custom board, and I am very confused. I would appreciate any support anyone could provide here.

I keep reading on other questions on this forum how the (official) nxp uboot-imx does not support SPL. I cloned what i think is the nxp uboot-imx from here:

git://source.codeaurora.org/external/imx/uboot-imx.git

branch=lf-5.4.y_v2019.04

When I look at the files for mx6sabresd, it sure looks like this version does support and build SPL by default.

Did the official nxp uboot-imx start supporting SPL or did i clone the wrong repo?

Thank you.

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
2,423 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Noorahmadshinwari

latest nxp uboot releases from source.codeaurora.org/external/imx/uboot-imx support spl.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,424 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Noorahmadshinwari

latest nxp uboot releases from source.codeaurora.org/external/imx/uboot-imx support spl.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
2,423 次查看
noorahmadshinwa
Contributor III

Hi Igor,

Thank you for your response.

I would appreciate it if you could have a look at my related question here:

https://community.nxp.com/message/1346580 

Thanks again!

0 项奖励
回复