Is MAC57D5xx OpenVG acceleration active with Free-RTOS ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is MAC57D5xx OpenVG acceleration active with Free-RTOS ?

1,002 Views
ravivarmanthiag
Contributor I

Hi,

I'm in charge of Implementing the GUI features using OpenVG in MAC57D5xx processor which runs Free-RTOS as operating system. In the internet i couldn't find the source of this MAC57D5xx  with OpenVG support which is compatible with Free-RTOS. Do we have any processor source code with Free-RTOS and OpenVG combined support. Because in the site i could only find openvg combined with either windows,android or Linux OSes.

Thanks.

0 Kudos
Reply
1 Reply

818 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ravivarman

I am not aware of Free-RTOS supporting this product, suggest to contact

local marketing as this part is marked as "Preproduction" and all its info is preliminary.

However seems gpu support is provided on below examples:

Software (1)

MAC57D5xxEVB Code Examples (REV 0)

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/mac57dxxx/mac57d5xx-devel...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply