Is MAC57D5xx OpenVG acceleration active with Free-RTOS ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is MAC57D5xx OpenVG acceleration active with Free-RTOS ?

1,424件の閲覧回数
ravivarmanthiag
Contributor I

Hi,

I'm in charge of Implementing the GUI features using OpenVG in MAC57D5xx processor which runs Free-RTOS as operating system. In the internet i couldn't find the source of this MAC57D5xx  with OpenVG support which is compatible with Free-RTOS. Do we have any processor source code with Free-RTOS and OpenVG combined support. Because in the site i could only find openvg combined with either windows,android or Linux OSes.

Thanks.

タグ(3)
0 件の賞賛
返信
1 返信

1,240件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Ravivarman

I am not aware of Free-RTOS supporting this product, suggest to contact

local marketing as this part is marked as "Preproduction" and all its info is preliminary.

However seems gpu support is provided on below examples:

Software (1)

MAC57D5xxEVB Code Examples (REV 0)

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/mac57dxxx/mac57d5xx-devel...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信