Is IMX8M Plus using WDQS?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Is IMX8M Plus using WDQS?

跳至解决方案
2,665 次查看
haryanl
Contributor IV

Hi all,

I am confirming whether the IMX8M Plus has the WDQS function enabled?
I checked the RPA excel file, but I don't understand clearly.
Can you confirm this for me?
1. If it is enabled then, use Mode 1 or Mode 2 as shown below (From DDR datasheet)
2. In the RPA file, where can Enable/Disable be confirmed?

haryanl_0-1717034852012.png

Thanks,

标记 (1)
0 项奖励
回复
1 解答
2,641 次查看
pengyong_zhang
NXP Employee
NXP Employee

Hi, @haryanl 

on i.MX8MP, we enable the WDQSEXTENSION feature of the DDR PHY whose description is as follows:

When set, DQS_T and DQS_C will be driven differentially to 0 and 1, respectively,
before and after a write burst, except during a memory read transaction.

From that I understand that DQS should be driven low at all times except a memory read transaction.

Here is measured the behavior of the system on 8MP EVK when WDQSEXTENSION is enabled and disabled:

pengyong_zhang_0-1717050378634.jpeg

 

 

在原帖中查看解决方案

3 回复数
2,635 次查看
pengyong_zhang
NXP Employee
NXP Employee

Hi, @haryanl 

Yes! You are right!

B.R

2,642 次查看
pengyong_zhang
NXP Employee
NXP Employee

Hi, @haryanl 

on i.MX8MP, we enable the WDQSEXTENSION feature of the DDR PHY whose description is as follows:

When set, DQS_T and DQS_C will be driven differentially to 0 and 1, respectively,
before and after a write burst, except during a memory read transaction.

From that I understand that DQS should be driven low at all times except a memory read transaction.

Here is measured the behavior of the system on 8MP EVK when WDQSEXTENSION is enabled and disabled:

pengyong_zhang_0-1717050378634.jpeg

 

 

2,629 次查看
haryanl
Contributor IV

Hi @pengyong_zhang ,

 

Thank for your reply.

in the RPA file, is it confirmed here?
By default it is set to enabled
haryanl_0-1717051794890.png

Because WDQS_Extension is used, is it correct that I understand that corresponds to DDR Mode 2: WDQS_on / WDQS_off definition based control?

Thanks,

0 项奖励
回复