Is IMX27 HSM (Hardware Secure Module) supported?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is IMX27 HSM (Hardware Secure Module) supported?

ソリューションへジャンプ
1,934件の閲覧回数
txh3157
Contributor I

Does iMX27 include hardware secure module (HSM) for factory to write X.509 cert/key? Is the SCC the right module to look into? If it is, how to enable it from Yocto BSP's setup?

0 件の賞賛
返信
1 解決策
1,922件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello txh3157,

The iMX27 does not include the HSM, The HSM is treated as a further core and can be full run controlled. Furthermore, common debugging of the Host/HSM cores and FLASH programming are possible on processor: MPC57xx and MPC56xx.

 

Regards

 

元の投稿で解決策を見る

2 返答(返信)
1,923件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello txh3157,

The iMX27 does not include the HSM, The HSM is treated as a further core and can be full run controlled. Furthermore, common debugging of the Host/HSM cores and FLASH programming are possible on processor: MPC57xx and MPC56xx.

 

Regards

 

1,913件の閲覧回数
txh3157
Contributor I

It is not possible for us to change schematic. In the iMX Linux reference doc, does these commands working in iMX27: sm_init_keystore, sm_detect_keystore_units, sm_establish_keystore etc under CAAM module? Can SCC module to be used by application?

Thank you!

0 件の賞賛
返信