Interfacing eDP with iMX6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Interfacing eDP with iMX6

ソリューションへジャンプ
3,234件の閲覧回数
mohammedazlum
Contributor IV

Hello,

eDP ( Embedded DisplayPort) will not support directly to iMX6 CPU. So we need to use a eDP converter/ bridge between the eDP and iMX6.

Please let us know that, whether FSL has tested the eDP with iMX6 ? If tested, could you provide the eDP converter part number ?

Regards,

Azlum

ラベル(4)
タグ(1)
1 解決策
2,372件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

HI Azlum

eDP is not supported natively in hardware, seems one can use

converter like DSI to eDP or similar:

PS8640,42 – MIPI Dual Channel DSI to eDP (paradetech.com/products/displayport-transmitters/ps8642/).

I am not aware of eDP usage with i.MX6.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
2,373件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

HI Azlum

eDP is not supported natively in hardware, seems one can use

converter like DSI to eDP or similar:

PS8640,42 – MIPI Dual Channel DSI to eDP (paradetech.com/products/displayport-transmitters/ps8642/).

I am not aware of eDP usage with i.MX6.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------