Interfacing WM8978 audio codec with imx6

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Interfacing WM8978 audio codec with imx6

1,219 次查看
shammi112
Contributor I

Hi,

Is there any reference document which explain connections between imx6 and WM8978 audio codec.

Regards,

SHAMMI

0 项奖励
回复
1 回复

992 次查看
igorpadykov
NXP Employee
NXP Employee

Hi SHAMMI

this depends which audio interface is used, please check SSI connections

description in AN2628 Programming Audio Applications

http://www.nxp.com/docs/en/application-note/AN2628.pdf 

or for SAI : AN4486

http://www.nxp.com/assets/documents/data/en/application-notes/AN4486.pdf 

ESAI : AN18148

http://www.nxp.com/docs/en/application-note/AN1848.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复