Intenet: Network configuration problem with IMX53

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Intenet: Network configuration problem with IMX53

2,436 次查看
Swamy
Contributor III

Hi All,


I have ported the internet browser and connecting to internet via wifi. I am facing a problem where in I am not able to resolve the name of any website.

Say, If I type google.com it will not work, but if type IP address of the google.com (http://173.194.66.94) it works.

In /etc/resolv.conf, I have even added the nameserver. Even I tried by adding some global ip address like 8.8.8.8, 8.8.4.4. But still no luck.

Please can anyone help in resolving this issue.

Regards,

Swamy

标记 (2)
0 项奖励
回复
2 回复数

2,334 次查看
Swamy
Contributor III

Hi Alexander,

Thanks for the reply. Yes I see that hosts:dns file is present inside the /etc/nsswitch.conf

Also, my /etc/hosts looks like

nameserver 192.168.43.0

Am i missing something else in the file?

Regards,

Swamy

0 项奖励
回复

2,334 次查看
Sasamy
Contributor IV

Hi Swamy,

verify that you can access to the DNS

$ grep "hosts" /etc/nsswitch.conf

for example

hosts:    files dns