Integrate LVDS for custom board for imx8qxpc0mek [ O.S Linux Yocto kernel -6.6.3 ] Nanbield.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Integrate LVDS for custom board for imx8qxpc0mek [ O.S Linux Yocto kernel -6.6.3 ] Nanbield.

644 次查看
Ram2
Contributor III

Hi NXP Team 

Need reference example for LVDS Display on M4 expersso SDK for custom LVDS display for imx8qxpc0mek
We need to example , can you please help us to integrate 

Custom Board : Imx8qxpC0mek [Hardware]
Linux Version :   kernel 6.6.3
SCFW : 1.15
M4 SDK : Xperesso 
Yocto version : Nanbield
Display :  LVDS [ LVDS display is connected via FPC cable between imx8qxp processor and Display ].  


Requirement:
We need to bring up the LVDS display from M4 once target gets turn ON with NXP logo.


How to proceed and where to look in to start any pointers or reference please help us on it.


0 项奖励
回复
2 回复数

596 次查看
AldoG
NXP TechSupport
NXP TechSupport

Hello,

For the SDK you may try with dpu driver examples located at <SDK installation path>\boards\mekmimx8qx\driver_examples\dpu

All documentation is available inside the SDK package at <SDK installation path>\docs

Also, note that we do not use an specific driver for a display we just write display timings and other configurations as you will see in all our examples.

You may download SDK from here:
https://mcuxpresso.nxp.com/en/welcome

Best regards/Saludos,
Aldo.

0 项奖励
回复

607 次查看
Ram2
Contributor III

Hi NXP Team,

Any update on below query?


标记 (1)
0 项奖励
回复