Integrate LVDS for custom board for imx8qxpc0mek [ O.S Linux Yocto kernel -6.6.3 ] Nanbield.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Integrate LVDS for custom board for imx8qxpc0mek [ O.S Linux Yocto kernel -6.6.3 ] Nanbield.

643 Views
Ram2
Contributor III

Hi NXP Team 

Need reference example for LVDS Display on M4 expersso SDK for custom LVDS display for imx8qxpc0mek
We need to example , can you please help us to integrate 

Custom Board : Imx8qxpC0mek [Hardware]
Linux Version :   kernel 6.6.3
SCFW : 1.15
M4 SDK : Xperesso 
Yocto version : Nanbield
Display :  LVDS [ LVDS display is connected via FPC cable between imx8qxp processor and Display ].  


Requirement:
We need to bring up the LVDS display from M4 once target gets turn ON with NXP logo.


How to proceed and where to look in to start any pointers or reference please help us on it.


0 Kudos
Reply
2 Replies

595 Views
AldoG
NXP TechSupport
NXP TechSupport

Hello,

For the SDK you may try with dpu driver examples located at <SDK installation path>\boards\mekmimx8qx\driver_examples\dpu

All documentation is available inside the SDK package at <SDK installation path>\docs

Also, note that we do not use an specific driver for a display we just write display timings and other configurations as you will see in all our examples.

You may download SDK from here:
https://mcuxpresso.nxp.com/en/welcome

Best regards/Saludos,
Aldo.

0 Kudos
Reply

606 Views
Ram2
Contributor III

Hi NXP Team,

Any update on below query?


Tags (1)
0 Kudos
Reply