Installing ROS on NXP i.MX8MPLUS-BB boards

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Installing ROS on NXP i.MX8MPLUS-BB boards

3,272件の閲覧回数
MAYIXIN
Contributor I

IMX8MPLUS-BB.jpgI already downloaded yocto on ubuntu,but I don't know how to Install ROS.

https://www.nxp.com/docs/en/user-guide/IMX_YOCTO_PROJECT_USERS_GUIDE.pdf 

0 件の賞賛
返信
2 返答(返信)

3,227件の閲覧回数
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @MAYIXIN,

I hope you are doing well.
 
One can refer to below mentioned post for installing ROS on NXP i.MX boards
 
Thanks & Regards,
Dhruvit Vasavada

3,253件の閲覧回数
khang_letruong
Senior Contributor III

Hi @MAYIXIN ,

There might be 2 possibilities at least, depending on your BSP version :

1. If you stay with pure Yocto image, you could inspire from the BSP of the iMX8M Plus AI Robot Platform : https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-%E6%9C%BA%E5%99%A8%E4%BA%BA%E5%B9%B...

2. You could also use Ubuntu based image and install ROS on the top of it. NXP Yocto offers possibility to bitbake Ubuntu image since Linux 5.10.9_1.0.0. See more here : https://community.nxp.com/t5/i-MX-Processors/I-MX8M-plus-AI-Robot-platform-Ubuntu-OS/m-p/1282237 or https://community.nxp.com/t5/i-MX-Processors/Yocto-build-fails-on-ubuntu-22-04LTS/m-p/1579880

Prior Linux 5.10.9_1.0.0, you have to generate the Ubuntu rootfs manually, but not recommended as the BSP might be too old for iMX8M Plus. For example : https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Build-Ubuntu-For-i-MX8-Series-Platform/t...

Hope this help!

Regards,
Khang

0 件の賞賛
返信