Installing Built Drivers on Yocto Image?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Installing Built Drivers on Yocto Image?

ソリューションへジャンプ
5,212件の閲覧回数
PaulDeMetrotion
Senior Contributor I

I have prebuilt some drivers for a RedPine wireless device and need to put the drivers and scripts onto a Linux image. I have created the following rs9113_1.0.0.bb recipe but I get errors when trying to copy the drivers. I do not get these errors with the scripts. Any ideas what I am doing wrong??

rs9113_1.0.0.bb:

DESCRIPTION = "Install of rs9113 drivers and scripts"

LICENSE = "MIT"

LIC_FILES_CHKSUM = "file://${COREBASE}/LICENSE;md5=4d92cd373abda3937c2bc47fbc49d690 \

                    file://${COREBASE}/meta/COPYING.MIT;md5=3da9cfbcb788c80a0384361b4de20420"

kmoddir = "/lib/modules/${KERNEL_VERSION}/kernel/drivers/net/wireless/redpine"

FILESEXTRAPATHS_prepend := "${THISDIR}:"

SRC_URI_append = " \

    file://onebox_common_gpl.ko \

    file://onebox_gpl.ko \

    file://onebox_nongpl.ko \

    file://onebox_wlan_gpl.ko \

    file://onebox_wlan_nongpl.ko \

    file://wlan.ko \

    file://wlan_wep.ko \

    file://wlan_ccmp.ko \

    file://wlan_tkip.ko \

    file://wlan_acl.ko \

    file://wlan_scan_sta.ko \

    file://wlan_xauth.ko \

    file://wlan_enable.sh \

    file://wlan_disable.sh \

"

do_install_append() {

    install -d ${D}${kmoddir}

    install -m 0755 ${WORKDIR}/onebox_common_gpl.ko ${D}${kmoddir}

    install -m 0755 ${WORKDIR}/onebox_gpl.ko ${D}${kmoddir}

    install -m 0755 ${WORKDIR}/onebox_nongpl.ko ${D}${kmoddir}

    install -m 0755 ${WORKDIR}/onebox_wlan_gpl.ko ${D}${kmoddir}

    install -m 0755 ${WORKDIR}/onebox_wlan_nongpl.ko ${D}${kmoddir}

    install -m 0755 ${WORKDIR}/wlan.ko ${D}${kmoddir}

    install -m 0755 ${WORKDIR}/wlan_wep.ko ${D}${kmoddir}

    install -m 0755 ${WORKDIR}/wlan_ccmp.ko ${D}${kmoddir}

    install -m 0755 ${WORKDIR}/wlan_tkip.ko ${D}${kmoddir}

    install -m 0755 ${WORKDIR}/wlan_acl.ko ${D}${kmoddir}

    install -m 0755 ${WORKDIR}/wlan_scan_sta.ko ${D}${kmoddir}

    install -m 0755 ${WORKDIR}/wlan_xauth.ko ${D}${kmoddir}

    install -d ${D}/etc/redpine

    install -m 0755 ${WORKDIR}/wlan_enable.sh ${D}/etc/redpine

    install -m 0755 ${WORKDIR}/wlan_disable.sh ${D}/etc/redpine

}

FILES_${PN}_append += " \

    ${D}${kmoddir}/onebox_common_gpl.ko \

    ${D}${kmoddir}/onebox_gpl.ko \

    ${D}${kmoddir}/onebox_nongpl.ko \

    ${D}${kmoddir}/onebox_wlan_gpl.ko \

    ${D}${kmoddir}/onebox_wlan_nongpl.ko \

    ${D}${kmoddir}/wlan.ko \

    ${D}${kmoddir}/wlan_wep.ko \

    ${D}${kmoddir}/wlan_ccmp.ko \

    ${D}${kmoddir}/wlan_tkip.ko \

    ${D}${kmoddir}/wlan_acl.ko \

    ${D}${kmoddir}/wlan_scan_sta.ko \

    ${D}${kmoddir}/wlan_xauth.ko \

    ${D}/etc/redpine/wlan_enable.sh \

    ${D}/etc/redpine/wlan_disable.sh \

"

Build Errors:

ERROR: QA Issue: rs9113: Files/directories were installed but not shipped

  /lib

  /lib/modules

  /lib/modules/kernel

  /lib/modules/kernel/drivers

  /lib/modules/kernel/drivers/net

  /lib/modules/kernel/drivers/net/wireless

  /lib/modules/kernel/drivers/net/wireless/redpine

  /lib/modules/kernel/drivers/net/wireless/redpine/wlan.ko

  /lib/modules/kernel/drivers/net/wireless/redpine/wlan_ccmp.ko

  /lib/modules/kernel/drivers/net/wireless/redpine/onebox_common_gpl.ko

  /lib/modules/kernel/drivers/net/wireless/redpine/wlan_tkip.ko

  /lib/modules/kernel/drivers/net/wireless/redpine/wlan_wep.ko

  /lib/modules/kernel/drivers/net/wireless/redpine/wlan_scan_sta.ko

  /lib/modules/kernel/drivers/net/wireless/redpine/wlan_acl.ko

  /lib/modules/kernel/drivers/net/wireless/redpine/onebox_wlan_nongpl.ko

  /lib/modules/kernel/drivers/net/wireless/redpine/onebox_wlan_gpl.ko

  /lib/modules/kernel/drivers/net/wireless/redpine/wlan_xauth.ko

  /lib/modules/kernel/drivers/net/wireless/redpine/onebox_gpl.ko

  /lib/modules/kernel/drivers/net/wireless/redpine/onebox_nongpl.ko [installed-vs-shipped]

0 件の賞賛
返信
1 解決策
3,417件の閲覧回数
madisox
Contributor III

Remove the ${D} prefix in the FILES_${PN} setting - that's why the packager isn't finding those files.

元の投稿で解決策を見る

2 返答(返信)
3,418件の閲覧回数
madisox
Contributor III

Remove the ${D} prefix in the FILES_${PN} setting - that's why the packager isn't finding those files.

3,417件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Paul DeMetrotion,

Are you still encountering this issue when installing the built drivers? The error seems odd. I think the _append suffix on the do_install, SRC_URI and FILES_${PN} may not be necessary.

In some forums I read that you may ignore the QA warning by using the following command, but it won’t fix the root cause so you may still be lead to an error.

INSANE_SKIP_${PN} = "installed-vs-shipped "

Regards,

0 件の賞賛
返信