Nitrogen6x2g Ubuntu kernel 3-14-52 : black screen
but display remains black!
What am I doing wrong?
Console:
non-CEA modes allowed on HDMI, audio may be affected
----------- trying to load /initrd.imgSolved! Go to Solution.
Hi,
As the blog post says:
This release uses the same mechanism as the 3.14.28 which means that U-Boot is in charge of setting the display parameters in the device tree. So it requires to use U-Boot v2015.07 or higher. Please make sure to read our blog post about this release:
What LVDS display are you using? Once you know its name, please find its match using:
=> fbpanel lvds
Once found, you can setup the display settings accordingly (here is an example for the hannstar LVDS display):
=> setenv fb_lvds hannstar
=> setenv fb_lcd off
=> setenv fb_hdmi off
=> savee && reset
Hope this helps.
Regards,
Gary
Hi,
As the blog post says:
This release uses the same mechanism as the 3.14.28 which means that U-Boot is in charge of setting the display parameters in the device tree. So it requires to use U-Boot v2015.07 or higher. Please make sure to read our blog post about this release:
What LVDS display are you using? Once you know its name, please find its match using:
=> fbpanel lvds
Once found, you can setup the display settings accordingly (here is an example for the hannstar LVDS display):
=> setenv fb_lvds hannstar
=> setenv fb_lcd off
=> setenv fb_hdmi off
=> savee && reset
Hope this helps.
Regards,
Gary
And that is what I was searching for!
I love you gary_bisson :smileyhappy:
Thank you for both answers!
Regards,
Laza