Install apt in Yocto

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
5,036件の閲覧回数
eugenephua
Contributor III

Hi there, i have managed to get imx6q to boot up using the files in L3.10.53_1.1.0_iMX6QDLS_Bundle. However, the yocto does not have apt command. May i know if anyone have managed to get it working?

Thanks!

ラベル(3)
0 件の賞賛
返信
1 解決策
3,067件の閲覧回数
jaymind
Contributor IV

Hello Eugene,

Plz check below link may it will help you....on same community

Regards

Jaymin D

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
3,068件の閲覧回数
jaymind
Contributor IV

Hello Eugene,

Plz check below link may it will help you....on same community

Regards

Jaymin D

0 件の賞賛
返信
3,067件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hello Jaymin D,

Thanks for your contribution to Freescale Community!

Best regards!

/Carlos

0 件の賞賛
返信
3,067件の閲覧回数
eugenephua
Contributor III

Hi Jaymin,

thanks for the info, i managed to load the debian root file system instead :smileyhappy:

0 件の賞賛
返信