Install LInux in i.MX6Q-SDB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Install LInux in i.MX6Q-SDB

ソリューションへジャンプ
4,756件の閲覧回数
joowonkim
Contributor III

Hi everyone

I'm beginner engineer.

So I feeling very difficult the i.MX6 board.

I boot i.MX6 board and apper Andriod screen.

By the way, I want install Linux in i.MX6 board.

How to delete android install the Linux.

I don't know nothing.

delete Android, install Linux.

teach me from the first.

please~~

Thank you to read.

P.S) I have i.MX6Q-SDB board

ラベル(4)
1 解決策
4,032件の閲覧回数
saurabh206
Senior Contributor III

Hi,

MFGTool  has "cfg.ini" file has different profile like "name = Sabre-SD".

All the profile described in mfgtools\Profiles\Linux\OS Firmware\ucl2.xml.

You can modified the ucl2.xml file and use your profile in cfg.ini file.

So You can use MFGtool in wondows8.

IF you have selected linux firmware than it will install linux firmware for you.

For simplicity you can use two different MFGtool for Android and Linux.

Thanks

Saurabh

元の投稿で解決策を見る

11 返答(返信)
4,032件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi JooWon

please read attached Linux Guide

Chapter 8 Using a Linux Host to Set Up an SD/MMC Card

and use demo files from link below for preparing SD card with Linux

L3.0.35_4.1.0_DEMO_IMAGE_BSP : i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite,

i.MX 6Solo and i.MX 6Sololite Linux Binary Demo Files.

L3.0.35_4.1.0_LINUX_DOCS

i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo and i.MX 6Sololite Linux BSP Documentation.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

4,032件の閲覧回数
joowonkim
Contributor III

Thanks you igorpadykov.

By the way, installed Android in i.MX Board

how to remove Android? and, read only chapter 8?

answer please~

By JooWon.

0 件の賞賛
返信
4,032件の閲覧回数
saurabh206
Senior Contributor III

Hi

JooWon

If you are booting from eMMC than please use MFGtool.

It will create partition and update required firmware for you on eMMC.

Other option is that you can boot the device from SDCard.

Prepare two SDCard one for Android and one for Linux.

Thanks

Saurabh

4,032件の閲覧回数
joowonkim
Contributor III

Thank you Saurabh Patel

If i use the MFGtool, in Window8 remove Android and install the ubuntu?

Everything the first time...

please answer.

Thanks

0 件の賞賛
返信
4,033件の閲覧回数
saurabh206
Senior Contributor III

Hi,

MFGTool  has "cfg.ini" file has different profile like "name = Sabre-SD".

All the profile described in mfgtools\Profiles\Linux\OS Firmware\ucl2.xml.

You can modified the ucl2.xml file and use your profile in cfg.ini file.

So You can use MFGtool in wondows8.

IF you have selected linux firmware than it will install linux firmware for you.

For simplicity you can use two different MFGtool for Android and Linux.

Thanks

Saurabh

4,032件の閲覧回数
joowonkim
Contributor III

Hi Saurabh Patel

Thank you 2 days ago.

I install the MFGTool, and I operating "cfg.ini"

By the way, I switched from Windows to Ubuntu.

I install the MFGTool, SDK Platform, UBoot.

Do you teach me installation Order?

please help me

Thanks.

0 件の賞賛
返信
4,032件の閲覧回数
saurabh206
Senior Contributor III

Hi

JooWon

Do you want to use MFGTool on Ubuntu development machine? Is there my understanding is correct?

Thanks

Saurabh

0 件の賞賛
返信
4,032件の閲覧回数
joowonkim
Contributor III

Hi

Saurabh Patel

Thank you reply.

Sorry to late reply (Now south korea lunch time)...

I want to the install Ubuntu on i.MX6Q Board.

At first, my desktop OS is Window8, But now OS Ubuntu.

The way I think, there is SDcard(8GB) in board and install the Ubuntu this SDcard(8GB)

How to install Ubuntu this SDcard(8GB)?

Sorry to bother.

JooWon,

0 件の賞賛
返信
4,032件の閲覧回数
saurabh206
Senior Contributor III

Hi JooWon

USB loader can be used for firmware update with linux development machine.

Please check following link.

https://community.freescale.com/docs/DOC-94117

Thanks

Saurabh

4,032件の閲覧回数
joowonkim
Contributor III

Hi

Saurabh Patel

Your answer is  been of help to me.

Thank you very much.

Ah! Sorry to bother....

Always gotta be happy!

Thank you!

JooWon Kim.

0 件の賞賛
返信
4,032件の閲覧回数
joowonkim
Contributor III

Thank you Saurabh Patel

Your help is very helpful to me.

I really thank you.

JooWon Kim

0 件の賞賛
返信