Input format for MIPI CSI in IMX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Input format for MIPI CSI in IMX6

1,340 Views
alpeshmandani
Contributor IV

Hello,

We are working on IMX6 dual processor for camera interface.

We need input format detail for MIPI CSI and which input format support by IMX6 dual

Can you please help me for above thread?

Thanks.

Regards,

Alpesh

Labels (1)
0 Kudos
Reply
1 Reply

1,209 Views
joanxie
NXP TechSupport
NXP TechSupport

I send the mx6d reference manual to you for reference, which offer the detailed capture format, pls refer to the Table 37-2. Data Formats Supported By The Camera Port.

http://cache.nxp.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf?fpsp=1&WT_TYPE=Reference Manuals&WT_VENDOR=FREESCALE&WT_FILE_FORMAT=pdf&WT_ASSET=Documentation&fileExt=.pdf

0 Kudos
Reply