eMMC pSLC mode support for i.MX25

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

eMMC pSLC mode support for i.MX25

Jump to solution
1,253 Views
yuuki
Senior Contributor II

Dear all,

We want to use eMMC memory with pSLC mode with i.MX25.

In this case, it is necessary for [156]PARTITIONS_ATTRIBUTE of Extended CSD Register to be programed

However, the eMMC I/F of i.MX25 is Specification Version 4.2.

We understand that Version 4.2 does not support this operation.

Can eMMC of i.MX25 support pSLC mode by software modification?

(Can [156]PARTITIONS_ATTRIBUTE of Extended CSD Register be programed by software?)

May I have advice?

Best Regards,
Yuuki

Labels (1)
0 Kudos
Reply
1 Solution
688 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yuuki

>(Can [156]PARTITIONS_ATTRIBUTE of Extended CSD Register be programed by software?)

yes, i.MX25 SDHC support such operation using CMD6 and this is described in

Table 23-30. Commands for MMC/SD/SDIO/CE-ATA Cards i.MX25 Reference Manual (rev.2, 1/2011)

http://www.freescale.com/files/dsp/doc/ref_manual/IMX25RM.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
689 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yuuki

>(Can [156]PARTITIONS_ATTRIBUTE of Extended CSD Register be programed by software?)

yes, i.MX25 SDHC support such operation using CMD6 and this is described in

Table 23-30. Commands for MMC/SD/SDIO/CE-ATA Cards i.MX25 Reference Manual (rev.2, 1/2011)

http://www.freescale.com/files/dsp/doc/ref_manual/IMX25RM.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply