Dear all
The previous mxc_ipudev_test supplied in BSP 10.04 contains a lot of very useful sample code and tests which are completely missing from the latest ipudev test. The newer IPU libraries are not completely compatible with the older ipudev tests, so I've made the necessary changes to the older version so it runs with the newer libraries and I've attached it here in case it's useful to others.
Original Attachment has been moved to: 177-1004mxc_ipudev_test.tar.gz
Is it possible to convert bayer format into some other formats using this test code ?