Info: Using older mxc_ipudev_test on newer BSP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Info: Using older mxc_ipudev_test on newer BSP

1,992件の閲覧回数
StevieRG
Contributor II

Dear all

The previous mxc_ipudev_test supplied in BSP 10.04 contains a lot of very useful sample code and tests which are completely missing from the latest ipudev test. The newer IPU libraries are not completely compatible with the older ipudev tests, so I've made the necessary changes to the older version so it runs with the newer libraries and I've attached it here in case it's useful to others.

Original Attachment has been moved to: 177-1004mxc_ipudev_test.tar.gz

ラベル(1)
タグ(2)
0 件の賞賛
返信
2 返答(返信)

1,373件の閲覧回数
ela_embedded
Contributor I

Is it possible to convert bayer format into some other formats using this test code ?

0 件の賞賛
返信

1,373件の閲覧回数
fcs
Contributor IV

Freescale doesn't seem to provide this code anymore, so many thanks!

0 件の賞賛
返信